AXIS#.PL.AINSCALE
Description
AXIS#.PL.AINSCALE is an analog position scale factor that scales the analog input (AINx.VALUE) for AXIS#.OPMODE = 2 , AXIS#.CMDSOURCE = 3 (analog position mode).
The value entered is the motor position per 1 V of analog input.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Rotary: counts/V,rad/V, deg/V, (Custom Units)/V, 16-bit counts/V |
Range |
+/- 4,398,046,511,104 counts/V
Specific unit ranges are adjusted to account for the above max count range. |
Default Value |
0 counts/V |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.PL.AINSCALE | 0x500C | 0x7 | DINT | - | Position | RW | False |
AXIS2.PL.AINSCALE | 0x510C | 0x7 | DINT | - | Position | RW | False |